This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005: Programming the IC

Part Number: CDCE62005
Other Parts Discussed in Thread: CDCM6208V1, CDCM6208

Hi,

I am using a clock synthesizer with part number: CDCE62005RGZT in my design to input a K2H processor. For optimizing board size, I am not planning to use any controller for programming it.

Can we get this part in which required output frequencies are pre-programmed in the EEPROMs present in the IC?

I need 156.25 MHz to be output in all the 5 outputs. If pre-programmed one is not available, is there any other fixed frequency parts which can be used for same purpose?

Thanks & Regards,

Madhu.