Hello
The HSDS outputs can drive the AC-coupled LVDS load as per Section 9.3.2.2 of the datasheet, while being configured for 4mA or 6mA current drive.
With 100 Ohm diff termination, taking 4mA, makes 0.4V diff voltage span at the load
However, Table 7.10 (page 11) provides Vod differential swing of HSDS at 4mA to me 958 mV typical.
How that correlate with each other ? What do I miss ?
Thanks in advance