This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVC1310: less number of outputs

Part Number: CDCLVC1310
Other Parts Discussed in Thread: CDCLVC1104, CDCLVC1103, LMK00804B, LMK00105

Is there a 3-4 output flavour of CDCLVC1310 also available?

  • Hi,

    CDCLVC1103 (3 outputs) or CDCLVC1104 (4 outputs) are similar devices with 3 or 4 LVCMOS outputs. However, these devices only accept LVCMOS input and are more limited in terms of output voltage range (only 2.5V and 3.3V LVCMOS are supported). In general, for the CDCLVC11xx family, the last two digits of the part number is the number of outputs. Devices are available with 2, 3, 4, 6, 8, 10, or 12 outputs.

    If a universal input is required, the LMK00105 and LMK00804B can also be considered.

    Regards,
    -Tim