This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK61A2-100M: Usual working temperature

Part Number: LMK61A2-100M
Other Parts Discussed in Thread: LMK04828

Is it usual that the oscillator is running at about 70°C with room temperature of 20°C with only a LMK04828 as load?

  • Are you using a thermal imaging camera to measure the hottest spot on the die, or a thermocouple on the top of the package?

    What is the PCB temp under the oscillator?  

    Did you follow the PCB layout guidelines and thermal considerations in the dataheet?

    Regards,

    Alan

  • We use a thermal imaging camera.

    The temperature at the bottom side of the PCB is about 50°C.

    The layout is quit similar to the Figure 18 in the datasheet. But what's shown there is not a good  thermal connection. If the GND pin is important for cooling I would place the vias around the pin.

    So as conclusion it's normal that the LMK61A2 heats up more than a usual oscillator and cooling has to be taken in account more than usual.

    Regards

    Ernst

  • Yes, I agree with your conclusion .

    Thanks,

    Alan