This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Noel,
David and I work on the same project, I tried the setting from the page 7, 8 and 9 but I didn't get any frequency output. I can only set a frequency by using the PLL tab. Below are the requirements and setting that we want to have. Please correct if need. Also to ramp I used the input RampClk and applied a 3.3V with a switch or with a function generator, nothing work.
Here are the requirement.
Below are the setting in the user control tab.
Beow is the setting in the Ramp limits tab.