Other Parts Discussed in Thread: LMX2572
I would like to know the actual loop filter values that are installed on the LMX2572 development board? The loop filter components documented in the LMX2572EVM Evaluation Instructions do not match what is actually populated on the EVM board. I just recently received the EVM board and I believe that the board is probably a newer revision than the version represented in the instructions.
The board I have has loaded components where the instructions call out DNP's and the resistors populated in the loop filter are different values from the documentation. In addition the board that I have is equipped with a 100 MHz crystal reference oscillator populated where the instructions say the board is shipped configured for external reference clocking.
Is it possible to get a schematic of the LMX2572EVM board as it is currently shipping, or alternatively just get the current loop filter component values as installed in the currently shipping boards.
Thanks,
Mark Schutzer