Other Parts Discussed in Thread: LMK04610, USB2ANY,
Hi,
The clock tree design for the system is planning to be implemented with LMK04610. The Kintex FPGA on board will configure the LMK04610.
But the option for programming LMK04610 with USB2ANY is also incorporated for easy debugging.
Please have a look at the doubts that follows
Q1. Why the level shifter CAVC2T45TDCURQ1 is connected between USB2ANY and LMK04610? Why is it given only on the STATUS1 pin and not in STATUS0 pin?
Q2. What is the voltage level of the signals available in the USB2ANY connector? Please validate the following
Pin 1= SYNC= 1.8V
Pin 2= SCSN= 3.3V
Pin 3= STATUS1= 3.3V
Pin 4= SDIO= 1.8V
Pin 5= NC
Pin 6= GND
Pin 7= RESETN= 3.3V
Pin 8= SCL= 3.3V
Pin 9= CLKIN_SEL= 1.8V
Pin 10= STATUS0= 1.8V
Q3. The FRC-10 pin cable from USB2ANY adaptor is connected to the socket JU1 on the Evaluation board of LMK04610.
From the schematic of USB2ANY (J4 on SNAU228) the 'pin6 is External 3.3V' and 'pin5 is ground' but it doesn't suit with the
pin mapping of JU1 connector on LMK04610 EVM as it has 'pin5 as NC' and 'pin6 as the ground'.
Both images are attached here.
That results in two things 'lack of common ground' and 'shorting of 3.3V supply inside USB2ANY'.
But it still working in EVM...
Do my observation are right? Elsewhere I miss the train?
Q4. If I adopt the same USB2ANY connection part with 'JU1 and CAVC2T45TDCURQ1' in my schematic, Can I use the USB2ANY module for programming the LMK04610 or is there anything more to keep in mind.
Thanks in advance
DEEPAK V