Other Parts Discussed in Thread: TLC555, LMC555
HI,
I am trying to build a simple cyclic pulse generator circuit using LM555. I want it to function as is shown in the attached image.
When the reset goes low i want the output to be stopped or set to a particular value and when the reset signal again goes high i want the switching signal to start with exact same frequency and duty cycle as before. The rising edge of the reset signal and the output should be synchronized.
I tried with a simple astable multivibrator circuit with the fixed duty cycle and frequency. When the reset pin is pulled low the output voltage sets at 2V, however when i again give high to the reset pin switching starts randomly. it takes 3 switching cycles by LM555 to go back to the original frequency.
Has someone faced this issue?
Can there be any other simpler way of achieving it? i was thinking about a small microcontroller maybe,