Hi all,
I attach the TICSpro log data below.
This is the log data after loading tcs file.
You can see that PLL1 RDIV reset and PLL1 NDIV reset is run a few time.
Is this step necessary?
When CLKIN is instability I set PLL1 register, PLL1 is unlock. However I reset it at PLL1_RDIV_SWRST or CLKIN_SWRST, PLL1 is locked.
Wrote Register R0x56 as 0x00 560A |
Wrote Register R0x56 as 0x00 560A |
Wrote Register R0x1B as 0x00 1B00 |
Wrote Register R0x1C as 0x00 1C10 |
PLL1 RDIV reset |
Wrote Register R0x57 as 0x00 5710 |
Wrote Register R0x1D as 0x00 1D00 |
Wrote Register R0x1E as 0x00 1E10 |
PLL1 RDIV reset |
Wrote Register R0x57 as 0x00 5710 |
Wrote Register R0x1F as 0x00 1F00 |
Wrote Register R0x20 as 0x00 2078 |
PLL1 RDIV reset |
Wrote Register R0x57 as 0x00 5710 |
Wrote Register R0x21 as 0x00 2100 |
Wrote Register R0x22 as 0x00 2278 |
PLL1 RDIV reset |
Wrote Register R0x57 as 0x00 5710 |
Wrote Register R0x61 as 0x00 6100 |
Wrote Register R0x62 as 0x00 6204 |
PLL1 NDIV reset |
Wrote Register R0x57 as 0x00 5718 |
Wrote Register R0x11 as 0x00 1101 |
Wrote Register R0x11 as 0x00 1100 |
Wrote Register R0x57 as 0x00 5710 |
Wrote Register R0x57 as 0x00 5700 |
Wrote Register R0x14 as 0x00 1401 |
Wrote Register R0x14 as 0x00 1400 |
Wrote Register R0x14 as 0x00 1402 |
Wrote Register R0x14 as 0x00 1412 |
Wrote Register R0x14 as 0x00 1402 |
Wrote Register R0x14 as 0x00 1402 |
Wrote Register R0x14 as 0x00 1412 |
Wrote Register R0x14 as 0x00 1402 |
Wrote Register R0x14 as 0x00 1402 |
Wrote Register R0x14 as 0x00 1412 |
Wrote Register R0x14 as 0x00 1402 |
Wrote Register R0x14 as 0x00 1402 |
Best Regards,
Sho