Other Parts Discussed in Thread: CODELOADER
hi ,
We use CPU on our own motherboard to control LMK03318 through IIC,
The HEX configuration generated using the GUI can get the desired clock,
but it can't be written to EEPROM.There is no clock output when power is down and then power on.
We follow ''10.5.4 Write SRAM '' and ''10.5.5 Write EEPROM''of datasheet.
but R136 register always is 0x1.
HW_SW_CTRL is H
GPIO[3:2] is HH
Is there any good idea to debug??