This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have two questions:
1- How LMK03318 compares with CDC7005 in terms of jitter performance?
2- Is there a tool that allows me to configure it? Or a software library of some sort?
To provide more context on Q.1 above, I need a low jitter clock source. I have a legacy project based on CDC7005 which performance is good. I am working on a new design that has similar requirements but based on more recent components and I am considering LMK03318 because or the LVDS interface support.
Clock requirements are:
Input: whatever works.
Outputs: 2 x 40MHz LVDS, 4 x 5MHz LVCMOS.
About the LVCMOS output, how does it affect jitter, system wise? Does using LVDS and a clock distribution IC provides any advantage?
Thanks in advance.
Hi, Lane,
First of all, thank you very much for your prompt response.
I will take a look at the documentation, thank you for the link. Also, thank you for the hint on table 8.26: the amount of information in the data sheet is overwhelming, it is pretty easy to get lost in the middle of it. :-b
I do not have the EVM. I tried to run CodeLoader anyway and it crashed with a code violation error. It would be great if it could run off-line (without the EVM) and showed and stored the configuration on a file to be used later.
I will accept your offer about configuration but first I will make the schematics to determine which output goes where. I will consider your comments about LVDS vs. LVCMOS jitter.
Once more, thank you very much for your support.
Elder.
About CodeLoader 4 error I mentioned above, the exact error is "Run-time error "6": Overflow" and then it quits. I am using Windows 10 64 bits.
I installed TICS Pro and it loads and works but has no support to LMK03318. It has support to LMK03328 though. How similar are they other than the second PLL?