This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am planning to use Xilinx ZC706 with TI based ADC and DAC EVM boards ADS5463EVM and DAC3152EVM for my design. I want my system to be clock synchronous (synchronized clock for ADC, DAC and FPGA board).
Can you guys suggest an external clock module/device which can give me 4 to 5 different 1 GHz/ 500 MHz clock outputs for the system?
Thank you,
VK
LMK04828 (LMK0482x family) is a popular jitter cleaner/clock generator with cascaded PLLs that supports the frequencies you need. There are many TI reference designs with data converters that use LMK0482x family: 
Alan