Other Parts Discussed in Thread: LMK04828, LMK04610, , LMK04616
We have a data converter we are using that was designed for use with the LMK04610’s 6-mA HSDS outputs that supplies the inputs for SYSREF and Clock SYNC on the converter. We need 13 total outputs, so we would have to use the LMK04616, but we were more interested in using the LMK04828-EP due to its smaller footprint and PLL2 available frequencies. The LMK04828-EP also has 6-mA HSDS outputs but the problem is that the VOH and VOL voltages between the two parts are very different and it does not seem that the LMK04828-EP VOH and VOL are compatible with this converter. Do you think there is anything we can do to get the LMK04828 or a similar part to put out the same outputs as the LMK04610?