Part Number: LMX2491
Hello:
I don't see direct guidance in the datasheet of the part about selecting loop bandwidth to support FM triangle wave creation. I do note that the triangle wave example is 20MHz peak to peak for a 1.5GHz carrier, with a triangle wave fundamental frequency of 20kHz.
Is it correct to assume here that the loop BW is much greater than 20kHz? Can general guidance be provided on how much wider the loop bandwidth should be than the maximum triangle wave frequency to be commanded?
Thanks,
Farron