This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04616: 8mA HDSD

Part Number: LMK04616
Other Parts Discussed in Thread: DAC38RF83

Hi

 

How can I connect an HSDS 4mA or 8mA (out clk from LMK04616) to DAC38RF83 that can receive ecl\lvpecl ?

Can I connect them with AC couple only or I need resistor termination?

At the data sheet of DAC38rf83 I have an example of only of ecl and pecl. I need to connect the LMK04616 to those inputs as DACCLK and SYSREF