Other Parts Discussed in Thread: USB2ANY,
Hi,
I'm currently using the FPGA board attached that has the LMX2582RHA clocking chip which I would like to configure with the TICS PRO Software. However, the SPI pins of the chip are not broken out to a header but are wired directly to the FPGA pins. Therefore, it seems the only way I can configure the chip is through the FPGA and I can not use the USB2ANY device. Consequently, how do I interface with the TICS PRO Software? If I flashed a USB to SPI design on the FGPA, would the TICS Software driver detect and work with the chip through the FPGA USB port? Or would I have to design my own programmer and if so is there more information on the programming method and protocol?
Thanks for any help in advance