This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572EVM: Using RAMP function for EMI frequency stepping

Part Number: LMX2572EVM
Other Parts Discussed in Thread: LMX2572

I have been asked by Customer Support - Case CS0171405 - to submit this question to E2E.
I would like to use an LMX2572 Eval board as a signal source for Electro Magnetic Immunity testing. I need to step from 800 to 3000 MHz in steps of 8 MHz, and dwell on each frequency for 5 seconds. Phase continuity or relationships are irrelevant.
I believe the RAMP function in TICSPro can be used to do this, but I'm not sufficiently familiar with the set-up process. I've looked at the procedures in the Data sheet (8.1.7) and the Eval board (3.2.2 and 3.2.3). I think this will be a Manual Ramp, but I did not see much reference to Manual Ramp in the Eval board document.
Would it be possible for you to give me the configuration values for the TICSPro RAMP menu, given the objectives above?
Thank you
regards,
Bob