This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ32000: power the RTC from main battery

Part Number: BQ32000
Other Parts Discussed in Thread: BQ24295,

Hi everyone, 

We are working on a new portable device that required an RTC and that will be powered by a non-removable rechargeable Li-On battery of 3.7v 3000mAh. The bq24295 will be used as power management and the tps63025 as the battery to 3v3 regulator. My question is, may I used the main Li-On battery as Vbat for the RTC instead of a coin battery? We would like to avoid using a coin battery due to many import and export restrictions on many countries of the products which contain these types of batteries. A supercapacitor is not an option since the device may be powered off for long periods of time.

I was thinking to connect the RTC Vcc to the 3v3 regulated voltage (from the tps24295) and the RTC Vbat somehow to the main battery (Vbat from bq24295). The problem with this is that the main battery voltage range between 3v and 4.2, which is higher than the Vcc 3v3.

Any suggestion you about this problem?

Regards.