Hello,
I recently got the eval board for part# CDCE62005 and installed the software and hooked it up. In playing with the part I have two questions:
1. My goal is to use CDCE62005 solely for its smart mux capabilities. I want both the primary and secondary reference to be 100 MHz and the output to be 100 MHz. In the case of the primary ref failing the secondary ref would automatically be switched to. The software doesn't seem to demonstrate that if I have the smart mux set to select pri ref then sec ref if I turn pri ref to 0 the output switches to sec ref. This may be because I don't actually have the CLK input and output hooked up, but as the input propagated to the output I would have thought it would be capable of switching as well. Even with the smart mux set to the secondary input I couldn't see it on the output. I was going to test this with real signals when I noticed problem #2.
2. With just the USB plugged in and the software running for about 10 minutes the chip became extremely hot to the touch and may have started to smell a bit. Is this because I was playing with the software without any CLK inputs/outputs hooked up? Or is there some other reason I am not seeing. I am running it using USB power only.
I know that was a bit convoluted but I appreciate the help! If anything needs clarifying just let me know!
Thanks,
Chris