Part Number: CDCEL913
Other Parts Discussed in Thread: CDCE913, , LMK1C1103
Hello expert.
I had QA in this thread. Then I have additional question for this.
I got answer that this device only support 32MHz or higher frequency input with LVCMOS mode.
Then, could this device's LVCMOS input support 3.3V LVCMOS output VCXO?
In regard to phase sync, Is there any solution to do phase sync with output?
For example change output port as Y2=72MHz and Y3=12MHz from the Y1=72MHz and Y2=12Mhz.
Also, could we sync at least 1 output signal's phase with input signal?
Best regards,
Kazuki Kuramochi