Part Number: LMX2595EVM
Other Parts Discussed in Thread: LMX2595, USB2ANY
Hi,
I'm having some unexpected issues with frequency drift when operating the LMX2595 EVM. I am using a high quality Wenzel oscillator at 100 MHz as my reference input (single ended) and attempting to get a 12.5 GHz output directly from the VCO.
However, when I attempt to measure the phase noise, there is an unexpectedly large amount of frequency drift (in the 10s of Hz) when measuring the phase noise. I am sure that it is not the Wenzel oscillator, as I have measured this separately and it performs as expected. I have not modified the loop filter on the EVM at all and the PFD is at 200 MHz (using the onboard input doubler.). The reference input power is around -3Bm.
Looking at the measured phase noise I have two observations (see below):
1) There are large fluctuations at <100Hz due to the previously mentioned frequency drifts. The phase noise analyser also warns me of the frequency drifts.
2) The phase noise power is around 10 dB higher in the reference section (<1kHz) than the expected (i.e. reference oscillator multiplied by 125^2).
I see similar behaviour at other frequencies. Any suggestions for what is happening here? Thanks.