This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE913-Q1: Propagation delay when PLL is used

Part Number: CDCE913-Q1

Hello Team,

I got some questions from customer about the CDCE913-Q1.

Q. How much propagation delay from VDD(1.8V) ramp up to start output clock?

Q. How much propagation delay from VDD(1.8V) ramp down to stop output clock?

[Condition]

VDD = 0V~1.8V, VDDOUT=3.3V, PLL is used.(NOT bypassed)

Input clock = 27MHz, Output clock =27MHz, 74.1774MHz

Thanks,

Yuta Kurimoto