The data line resistance values for R5, R8, R9, R16, R19, R20, R22 are all 12Kohm, which I'm trying to understand. With the input capacitance of the digital input pins, I would think this would limit the max bus speed.
The EVAL board is running quite slow so no problem here of course, but to meet the 75MHz speed I think this would be a problem.
Could you recommend a different value, or the inclusion of an integrated RC filter with ESD protection like the NUF6406MNT1G , AOZ8175DI or similar?