Other Parts Discussed in Thread: LMK61PD0A2, LMX2595
Hi
I have a question about LMX2595EVM. We are trying to use LMX2595EVM to generate 400MHz clock. We are using external clock for reference clock and its frequency is 100MHz.
However, we saw different behaviour using different 100MHz reference clock. In this case we used 1) Wenzel (100MHz, sine wave) and 2) LMK (LMK61PD0A2, which is embeded on LMX2595EVM control board, 100MHz square wave). We compared the phase noise of 400MHz clock generated by LMX2595EVM and the result is shown below.
We found that even though 100MHz Wenzel (blue) has much lower phase noise than 100MHz LMK (orange), the phase noise of 400MHz triggered by Wenzel has lots of spurs and 400MHz generated by LMK looks very clean.
The measured waveform of two 100MHz reference clock is shown below. The measured peak-to-peak voltage of Wenzel and LMK are 400mV and 800mV, respectively (which is above the minimum required voltage for LMX2595).
The LMX2595 PLL setting is also attached.
Can you help us solving this problem? We are expecting 400MHz generated by Wenzel should be better than LMK because 100MHz Wenzel has better phase noise. However, we are not sure where the spurs in phase noise measurement come from. Is there any way to remove the spurs?
Regards
Zichuan Zhou