Part Number: TSW1405EVM
Hello,
I'm using the TSW1405 capture board with the HSDC Pro to capture data from the ads5474 parallel LVDS output ADC, I can't get the SNR and ENOB values of the ADC as described on the datasheet, the values I get are too bad (ENOB = 2 bits while I should get 10 or 11 bits ).. And I think this is due to the glitches I have on the codes, that must be caused by some defect in the digital section ( hardware or firmware ? ).
Attached are snapshots that show the SNR and ENOB when using a sampling frequency of 200 Msps and an input frequency of 50 MHz:
then with an input frequency of 700 kHz to reconstruct the sine wave and show the glitches on the codes:
I need some help to remove those glitches.
I also can't find the whole code for sample wise adcs..
Thanks in advance,
Best Regards,
Ayoub,