Other Parts Discussed in Thread: TMP235, TLV2553
We're seeing what appears to be the same issue that is referred to in this posting:
Power cycles with a short time off (1-3 seconds) result in corrupt data on some TLV2556 channels. Power cycles with a longer off time (>4 seconds) yield normal operation with no corrupted data. A few notes about our application:
- The SPI bus is connected to an FPGA
- We're operating with all 11 channels in 12-bit unipolar mode
- We're using a 2.5V external reference
- ADC inputs are a combination of:
- Temperature directly from a TMP235
- Power supply voltage monitors consisting of a resistor divider with a capacitor to ground from the center of the divider
- 10k OHm thermistor resistor divider
- The FPGA, ADC, and 2.5V reference are all powered from the same 3.3V rail
We've added drain resistors to all power waveforms and verified that all voltages are being drained to near zero volts during the off time, but the problem still persists. Is the root cause of this issue known? Is there a fix to support shorter power cycle times?