Hello,
I have read the datasheet and all threads regarding this device here in this forum. However, I am not sure whether I initialize the device in a correct way.
1) Can I write the values for my application as default register values or do I have to write the baseline values in the datasheet first?
2) Do I have to write all (all writeable register; note that 0x07 and 0x3e are read-only as I understood) registers in increasing order?
3) Or should I write them in decreasing order to fulfill the the note in the datasheet saying "Write the Clock Monitor (0x09) register after the Test & Scan Control (3x0D) register".
4) Should I really write all reserved and not-used registers or are there further register that should not be written (except 0x07 and 0x3e)?
Best Regards
Kristian