Other Parts Discussed in Thread: ADS1282
Dear all,
I have some question about Power-ON Reset and HW reset.
1. Datasheet reports that at power-up, ADC removes internal reset after Trst = 2^16/Fclock, then first data is output after Tdr = 63/Fdata.
Since ADC starts in FIR Mode with Fdata = 1000SPS and my Fclock = 4MHz, Trst =~16ms and Tdr =~ 64ms.
2. Datasheet reports that Tdr = 63/Fdata after hardware reset by nRESET pin cycling.
My questions are:
- Is, in case 1, possible to do any operation, including synchronizing, configure or calibrate the ADC just after Trst without waiting for first nDRDY negative edge (i.e. Tdr)?
- Is, in case 2, possible to do any operation, including synchronizing, configure or calibrate the ADC just after Trst without waiting for first nDRDY negative edge (i.e. Tdr)?
- Does the ADC starts converting just after either power on reset or pin reset removal and consequently be possible to retrieve converted data upon the first occurring nDRDY negative edge?
- Does power-on reset or pin reset require SPI reset before sending commands to the ADC or retrieving conversion data?
Datasheet says SPI is reset by holding SCLK low for 64 nDRDY periods. Does it means Tspi_rst = 64/Fdata? (after reset removal it would be 64ms).
I'll thank you in advance.
Daniele