Other Parts Discussed in Thread: DDC264
Hi
I'm using DDC264EVM and I have some question.
1. i connected just one sipd to the point that it was shown in picture below and also connected pin 1 to pin 2 of jumper 10 to read the data. as you can see in this picture, 25 resistors series to the input pins of ddc264.
my question is that, the value which i read in the software is correct value or i have to multiply it by 25. because i assumed the amount of current that produce by sipd is divided into 25 parts (25 input of ddc).
2.we used ddc264 ic in our customized board. the amount of offset that we measure in our experiment is about 3100 which is different from the amount that you mentioned in link below (4095).
my question is that, is there any negative swing in our experiment which is affected our offset value or this is normal to read this amount of offset.