Part Number: THS5641A
Other Parts Discussed in Thread: LMH6601, LMK04828
Hello,
Could you review the schematic with THS5641A?
The circuit design is on Sheet 17.
Thank you,
Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Andrew,
1. Suggest adding series 22 ohm resistors and or a buffer to the data lines if the traces are long from the FPGA. Same for the CLK driver.
2. Add a 4.7uF and 0.1uF decoupling caps to AVDD pin 24. Place these and C332 close to the pin.
3. Add bulk 10uF decoupling caps to both AVDD and DVDD.
3. Make sure all digital inputs meet the digital specs on sheet 6 of the data sheet.
Regards,
Jim
Jim,
I think I have addressed all of your comments.
In addition,
Please let me know of any additional feedback.
Regards,
Andrew
Andrew,
1. I think you need to adjust the supplies on the LMH6601, as per the data sheet, V+ - V- must be no greater than +5.5V.
2. Place R321-R329 as close as possible to the FPGA.
3. The DAC performance may be reduced if the clock from the FPGA is noisy. Most customers do not use the FPGA for a clock source.
Regards,
Jim
Hi Jim,
In terms of coupling between THS5641A and LMH6601, I have a resistor to the ground. Now I am thinking I need a filter for anti-aliasing. Perhaps this would be question for LMH6601.
Thank you,
Andrew
Hi Jim,
I'm going to close this case, and open a new case for the amplifier separately.
Thank again for your support.
Regards,
Andrew