Part Number: ADC12DJ5200RFEVM
Hello,
ADCxxDJxx00RF EVM GUI, I can see SERDES PLL Locked LED is green.
This PLL status follows the ADC sampling clock from the external RF signal generator.
But SYNC STATUS and LINK UP LEDs are dark green.
This status means I can't read SerDES output data.
How to debug the point to make ADC LINK UP?
My setup is as follows:
JMODE 31
FPGA reference 125 MHz
External Fs 2500 MHz
SerDES rate 8250 MHz
At the FPGA side:
Core clock 124.751 MHz
GTY rx user clock 124.751 MHz
Sysref 3.906281 MHz
FPGA GTY IBERT measurement 7.997 Gbps
Thanks,
Kiman