Hello!
We are designing an opto-electronic device and we have chosen the DDC232 as an ADC to read data from a photodiode array.
I wanted to ask if it is possible to use the same microcontroller SPI peripheral for configuration and data readback (we are using only one DDC232 so we do not need DIN pin):
- SPI MISO -> DDC232 DOUT
- SPI MOSI -> DDC232 DIN_CFG
- SPI CLK -> CLK_CFG & DCLK
Studying the datasheet it seems that configuration phase stops after CONV pin is strobed, so I wanted to ask you what happens if we keep sending clock signal on CLK_CFG pin.
I have seen this same question asked 4 years ago with no clear answer, but maybe there is un update by now
Thank you very much
Guido