Other Parts Discussed in Thread: TMDSEVM6678, ADS8681
hello,
I am searching for a DSP and ADC EVM for demodulating analog signals in real time in the lab. For the DSP development board I would like to use the TMDSEVM6678EVM, which has an 80-pin expansion header that should allow the ADC to be connected.
For the ADC, a 14Bit resolution and a 2MSPS sample rate is desirable. I think the ADS8681EVM-PDK definitely meets my requirements, but this ADC EVM does not seem to connect directly to the DSP board. The interface of PHI controller seems to be 60-pin. Should I buy an additional expansion board. Or maybe you can suggest me another ADC EVM that can be connected to the DSP board.
Thanks for the help.