Other Parts Discussed in Thread: ADS1298
Hi,
Iam trying to establish a SPI communication between ADS1298ECG to Arduino UNO.
ARDUINO CONNECTION WITH ADS 1298 ECGFE BOARD
J3.3 SCLK connected to Arduino pin 13
J3.4 GND connected to Arduino pin GND common.
J3.7 CS complement connected to Arduino pin 10
J3.8 RESET connect to Arduino pin 4.
J3.11 DIN connected to Arduino pin 11
J3.13 DOUT connected to Arduino pin 12
J3.15 DRDY connected to Arduino pin 3 (programmed)
J4.9 power supply is 3.3V
J4.5 connect to Arduino GND
I also connected the J4.10 power supply is 5v of the arduino.power supply 5v.
But when MEASURING J4.10 iam getting 5v, bt the TP7 ,IAM NOT GETTING ANY VOLTAGE. similarly is the case with the TP5,TP13,T6,TP9. Also Iam trying to read the control register ID of ads298, bt iam getting the value as 0. Can you help me solve this issue??
waiting for reply
Thanks
Neelima S