This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1013-Q1: ADS1013-Q1 VOH value

Part Number: ADS1013-Q1


Hi Team,

Q1: Please check ADS1013-Q1 have VOH value.

Q2: DVDD is Max or Min for VOH value?

Thank you so much.

  • Hi Lee,

    Maybe you need to better understand the I2C protocol and how I2C functions.  The SDA line is open-drain and is not active push-pull.  The open-drain is pulled high (with a resistor) to VDD as per protocol.  So there is really no VOH as there is no active driver and that is why it is not specified in the datasheet.  The logic high voltage is strictly related to the VDD supply voltage.  There is no min or max just VDD.

    Best regards,

    Bob B