This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1333M10: An Isolated ADC - (To sense 0 to 10V input voltage)

Part Number: AMC1333M10
Other Parts Discussed in Thread: AMC1210, ADC161S626, OPA2388-Q1

Hello,

Could you please confirm if the isolated ADC AMC1333M10 is suitable for processing a 10V analog signal with a frequency range of 1-5 Hz? If not, kindly recommend an alternative isolated ADC that would be more appropriate for this application.

Additionally, I would appreciate your guidance on selecting a suitable OpAmp for the aforementioned setup.

Please consider the following property of ADC and DAC as follows:

An Isolated ADC  - (To sense 0 to 10V input voltage)
   
Sampling rate - 200ksps or 250ksps
Resolution - 12 bits
Isolation can be in ADC or ADC front OpAmp
Channels - preferable 4 Independent
Simultaneous sampling not required
 
Kindly suggest if "AMC1210 Q1" part is suitable for this. 
 
An Isolated DAC  - (To Drive 0 to 10V input voltage)
 
Sampling rate - 200ksps or 250ksps
Resolution - 12 bits
Drive current - up to 250mA to 300mA
Channels - preferable 4 Independent
Isolation can be in DAC or DC Driver OpAmp
Thanks