This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4490: AFE4490 LED no woring

Part Number: AFE4490
Hello, I tried to use afe4490 to measure spo2, but the LED light did not light up during the implementation. 
I have powered on the afe4490 and written it into the register, but it still has no effect.I've seen similar posts before, but I couldn't find the answer.
The LED I use has a common anode and is supplied with a voltage of 3.3v externally.
The other end of the LED is directly connected to the TX pin. When I do not connect the LED, the single TX pin is 0.99V and 3.3V. No voltage between TX and TX
The following is my schematic, the MCU is ATmega328PU