Other Parts Discussed in Thread: DAC39J82
Greetings,
We got a DAC39J82EVM evaluation board, and are trying to use it for arbitrary pulse generation using the ZCU102 xilinx board. I've noticed in other forum questions that Xilinx's board do not have the F10/F11 pins routed to the FPGA, and so the Sync signal has to be routed through another GPIO port. From checking the DAC39J82EVM schematic, I don't see how the sync signal can be connected to the J21 port of the board (also recommended in those forum questions). How can I connect the sync signal between these two boards?
Thanks,
Matías.