Other Parts Discussed in Thread: ADS1247
Hi,
I'm trying to obtain valid A/D data from an ADS1247 interfacing a 4 wire PT100, but I can't obtain stable data (it change every sample and it doesn't seem related to my scenario).
My hardware setup is almost the same the one reported in TI AN SBAA180, paragraph 5. The only exception are:
- AIN0 as IDAC1 current generator;
- AIN1 and AIN2 used to connect line2 and line3
- Only one power source for bot AVDD and DVDD from a 3.3V battery (it's a wireless sensor based on TI CC1110-F32)
Basically, it's this hardware setup from another TI document:

I can correctly write and read from registers, so I don't think that is a problem related to SPI bus.
My registers configuration is the following:
- MUX0 = 0x11
- MUX1 = 0x20
- IDAC0 = 0x7
- IDAC1 = 0xF
- SYS0 = 0x70
Can someone help me to understand where I'm going wrong?
Thanks a lot,
Carmine


e