This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS122C04: I2C hang occasionally

Part Number: ADS122C04


Tool/software:

I have worked with this device on 4 different applications, device works well.

The problem is that my newest application hangs up occasionally when I write to a register or acquire data. There is one main difference with this application: I am in this case outputting a current source from the chip.  All functioning circuits that use this chip are identical electrically and are controlled the same way.

The only differences between them are the register settings.

 

  • This is an example of typical register values I initialize when things work properly.

Register 40h = 0xB1, set input configuration, no gain

Register 44h = 0x00, default to 20 SPS, single shot mode

Register 44h = 0x00

Register 4Ch = 0x00

 

  • When I use these register settings I get the occasional hangs.

Register 40h = 0x72, set input configuration and X2 gain

Register 44h = 0x48, set at 90 SPS, single shot mode

Register 44h = 0x01, set current source to 10ua

Register 4Ch = 0xA0, set REFP as DAC1 current source output

 

Again, the circuit works fine, we sample once every second or so. The I2C hang is maybe 2-3 times during an 8 hour period of run-time.

 

Any thoughts on this issue?