Tool/software:
HI
I have a problem with my PAMB. It doesn't pass the step of updating firmware.
When I connect to the software online, I have a first message :
and then i waiting all the time with this message:
The board is connected and the drivers intallation is done.
Help me, please
Regards
Hello Willy,
Thank you for posting on TI's E2E forum!
I will note this FAQ and an additional PAMB related post for future use even though it seems like you might have already tried these:
[FAQ] How do I resolve PAMB EVM connectivity and/or driver installation issues
BOOSTXL-ADS7142-Q1: GUI Initial Setup. PAMB not detected
Does the GUI hang with the "Firmware update in progress"? sometimes updating the firmware takes some time and I just want to confirm that waiting long enough is not an issue.
If you press "Cancel" in the "DFU Device Detected" window and then go to "File" in the top left corner, are you able to select "Program Device" and follow the instructions in the second link above? Does this work?
Otherwise, I would suggest manually resetting and re-flashing the firmware into the PAMB controller: Downloading Firmware to the PAMB
Re-downloading the firmware should fix this issue, but please let me know otherwise.
Best regards,
Yolanda