Hello to everyone,
I am writing here in order to ask some information about the interfacing of the DAC34SH84 Evalutation module, to my FPGA board.
Basically what I would like to do is to generate two output signals with my FPGA and send them to the next device. The problem is that I woul like to generate two high frequency signals and send them separately. I woul need the DAC/DACs to work with 1.5 GSPS on both channels. I admit that is the first time that I actually deal with hardware, and in this meaning I would need a little help to find out how I can interconnect all my devices.
So the questions are:
1) Can I reach, with the DAC34SH84 Evalutation module, this sample speed?
2) Would it be possible to reconstruct both the input signals and send them separateli on the output channels, is the interleaving working for both channels? (as each channel comes out with 750 GSPS)? Or should I use two separate refencence boards in order to obtain those results?
3) In case I need two Ref. Boards, on my FPGA Dev board I have 2 HSMC connectors, would I have the opportunity to connect both the DAC Boards to it? In your experience do I need some adapters?
Thank you in advance for your help and consideration.
All the best,
Giovanni.