This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hellow
I Request Configuration Files for ADS54J42 Device.
LMFS : 4211 & 4244
Sampling Rate : 600MSPS.
Decimation : Not Use.
Best Regards.
Louis,
The files are attached.
Regards,
Jim
Low Level ADS54J42_LMF_4244.cfgLow Level ADS54J42_LMF_4211.cfg
Hi jim
Thank you so much.
This is ADS54J42 Test Source.
set5469(sel,0x000000,0x81); // Total Reset (self clearing)
set5469(sel,0x800059,0x20); // PERF MODE set
set5469(sel,0x6800f7,0x01); // Digital Reset(self clearing)
set5469(sel,0x680041,0x00); // DEC_En, DecFilt Mode(Lowpass Filter)
set5469(sel,0x68004D,0x00); // DEC Enable
set5469(sel,0x680052,0x80); // Dx_bus Enable, LSB Digital Gain Enable
set5469(sel,0x680072,0x08); // Dx_BUS Enable
set5469(sel,0x68004B,0x00); // 2' complement
set5469(sel,0x680000,0x00); // After Digital Configuration, Reset Togle '0' --> '1' --> '0'
set5469(sel,0x680000,0x01); // After Digital Configuration, Reset Togle '0' --> '1' --> '0'
set5469(sel,0x680000,0x00);
set5469(sel,0x6A0016,0x02); // JESD PLL MODE(20X/40X) Mode
set5469(sel,0x6A001F,0x80); // Software fix 2016-11-17 오후 3:33:04 ti recommand code
set5469(sel,0x6A0000,0x08); // Software fix 2016-11-17 오후 3:33:06 ti recommand code
fpga_set_spi(sel,0x400501); //set this to do only one channel write
fpga_set_spi(sel,0x600820); // only for channel A
fpga_set_spi(sel,0x400500); // clear to broadcast writes to both channels
set5469(sel,0x690001,0x02); // 4Lane Mode
set5469(sel,0x690000,0x80); // JESD Digital, K_en, TestEn, FILP ADC Etc
set5469(sel,0x690005,0x80); // Scramble Enable
set5469(sel,0x690006,0x0F); // JESD Digital, MultiFrame(K) Set
set5469(sel,0x690031,0x0A); // JESD MODE(20X/40X)
set5469(sel,0x690032,0x0A); // JESD DB bus Reordera
Please Check the Source for 4244 mode.
Best Regards
Hi Jim
My Customer is Testing with the config file your sent.
I Check the testing results.
I will request you again when an issue occur.
thank you.
Regards.