Other Parts Discussed in Thread: DXP, DAC9881, USB2ANY
I have tried to test the EVM board on 2 different computers, running Win 7 x64.
As per user guide, I installed DXP 2.0.0 before plugging the usb connector. I can see the VISA driver on Device Manager whenever I plug or reset the board.
NI-VISA driver is 1.0.0.
However DXP always says:
When I launch the utility, it can't download the file:
Also, DXP user guide says that "When the DXP application is loaded, the driver will change from the NI-VISA to a WINUSB driver that appears as DXP in the Device Manager, shown in Figure 9." This step does not happen.
I am using the power supply that came with the EVM, and I am using the board as it came - didn't change any jumper. I have tried with 2 different USB cables, and at least 4 different USB ports.
If this information helps, I have not connected any external analog power supply so far. MMB0 is rev. D, and BOM is rev. E. I have also tried to run DXP in compatibility mode.
Also, I have Labview 2016 installed on both computers.