Other Parts Discussed in Thread: , LMK04828
Hi,
we are evaluating DAC38RF82 with DAC38RF82EVM+ZCU102. The only hardware modification I made is soldering R10 onto the EVM board to use the single-ended SYNC~ signal. We use the Xilinx JESD204 IP core to talk to the DAC.
Attached our EVM .cfg file. We use clock mode 4: on-board VCXO clock mode. LMK PLL VCO1 set to 3072MHz, FPGA device clock=192MHz, DAC device clock=122.88MHz, sysref=19.2MHz, Fdac = 6144Msps, Linerate=7680M, DAC on chip PLL mode, Dual DAC, single link, real, LMFSHd = 82121,4x Interpolation, DAC PLL settings M = 25, N = 2. We use the same settings for both DAC A and B. It seems that DAC B is not working properly.
In the FPGA we first set DAC A and DAC B to the same sine wave data flow. As showed in Fig1, we can get correct output (24MHz) from DAC A, but weird signal out from DAC B. Both DACs generate stable signals.
Then we changed the sine lookup table step size to 2 for DAC A to output 48MHz, and set DAC B for a 192MHz square wave. Fig2 shows what we got. The signals seem to be correct (at least for the frequency). But they are not stable, the signals stop frequently as showed in Fig3.
Attached also the verilog file for signal generation. I also checked the FPGA pin assignment, they should be right.
Could you please help us with this case? Thanks in advance!
Best,
Han
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/73/files.7z
Fig1:
Fig2:
Fig3: