Part Number: DAC7678
Hello,
I don't know if this question could be related to this one, but the datasheet is quite confusing on this matter.
I am trying to read out the power down status of each channel, with the read command described on Table 18.
Here is a dump of this register after the following steps :
Disabling all DACs with 100kΩ pull-down
0x02FF
Enabling DAC E
0x0010
Enabling DAC C
0x0004
Disabling DAC E with 100kΩ pull-down
0x0210
It seems to me that the register only echoes back the last power command received.
Is it the expected behavior ?
Thanks