Ref doc: SNAS621A-June 2013-Revised December 2014
Loop powered schematic:
- When DAC is in Loop-powered mode (Figure 15)
The loop instrument and the DAC grounds are isolated. Even though the potential across loop supply and it's own ground is 5V, the potential difference at the input of the voltage regulator and it's ground (LM2936MP-3.3) is less than 3V, so the DAC is not even powered ON.
- When DAC is in Self-powered mode (Figure 16)
If we try to output current greater than 16mA, we get a loop error.
How to resolve these issues?