Part Number: ADS1263EVM-PDK
Other Parts Discussed in Thread: ADCPRO, ADS1262, ADS1263
Hi,
I am having an issue with the evaluation board ADS1263EVM-PDK and the ADCPro software. The evaluation card is us to make a proof of concept for a medical device. There is three electrodes that are connected to IN2, IN3 and GND terminals.
Each time I use the electrod and sampling some data like my heart beat, I am always getting a PGA negative rail fault even if the data is between the PGA rails.
The evaluation card is supply in bipolar (±5V) and the internal reference is used.
The ADCPro is setup for sampling AIN2 and AIN3. The PGA Gain is set to 1V/V.
The sampling data magnitudes are between 3.9mV and 4.7mV.
If I use a signal source, I am able to sample a DC signal from -2.2V to +2.2V without the negative rail error.
I have attached the sampled heart beat signal exported to an excel file.
Any idea?Heart beat.xlsx
Thanks
Olivier Bergeron