Part Number: ADC12DJ3200QML-SP
Other Parts Discussed in Thread: ADS5400, ADS54J20, TSW14J57EVM, TSW14J50EVM, ADC12D500RF
Hi,
I need advice to select a part and EVM.
I am looking for a prototype LIDAR system. Minimum ADC Which I am looking is 1 Ghz and 12 bit. I prefer Intel Altera FPGAs to communicate this ADC. Sometimes TI offers 2 EVM ( one for ADC and one for FPGA board) Or TI offers a single board EVM which includes ADC and FPGA together.
I am looking for a cost effective solution.
Ideal system Which I am looking for is Highest ADC with multiple inputs channel on EVM at the same time When I want, I would like to use a single channel with High sampling frequency. Like if you have 6GHZ ADC, is there a possibility Which I can use 6 channel at 1 GHZ or a single Channel 6 GHZ option.
Second, FPGA companies provides High END and Low END like Arria FPGAs(High END) and Cyclone 10 GX FPGAs(Low END). But Cyclone 10 GX have also a very high end high Speed IOs. The advantage of Cyclone 10 GX FPGAs is that Their tool support ( Quartus Prime) is free.
At the end, I am looking for your best device with Minimum cost with multiple use cases.
In short, do you have a solution described above with your high speed ADCs with minimum cost for prototyping at the same time offers multiple channel minimum 1 ghz 12 bit with FPGA board included or together?
Thanks and best regards,