Hi,
I would like to set up registers by below methods, could you please answer my questions?
1.Are methods for "initial register setting" and "update DAC output" true?
2. In initial register setting, Which is wait time "1" , 50ns or 2.4us?
3. In initial register setting, Which is wait time "2" , 50ns or 2.4us?
4. In update DAC output, Which is true , No.1 or No.2?
Best Regards,
Nishie